Glass for Wearables | Scratch Resistant Smartwatch Glass | Corning Gorilla Glass
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
IE is bad

Close[x]
Smartphones

Gorilla Glass Applications

Gorilla Glass Applications

Smartphones

GORILLA® GLASS FOR WEARABLES AND SMARTWATCHES

Providing superior damage resistance and touch sensitivity, it’s not surprising that Corning® Gorilla® Glass has been used on more than 5 billion devices. And over the last few years, a growing number of those devices are coming from the wearables market. As wearable technology has evolved from a fitness aid to full-fledged smartwatches, leading manufacturers are turning to Gorilla Glass to provide their wearable devices with the ultimate combination of damage resistance and performance; and for good reason. All around the world, consumers are putting their wearables to the test. From athletic pursuits to just making it through the day, an improved ability to survive the potential bumps, knocks and scrapes is essential. Recently introduced, Gorilla® Glass DX and Gorilla® Glass DX+ are two new glass composites from Corning that feature an anti-reflective property to vastly improve optical clarity under bright light, while maintaining the legendary toughness and touch sensitivity of Gorilla Glass. Tough and tougher, Gorilla Glass DX and Gorilla Glass DX+ represent a new era of wearable elegance with durable, nearly invisible surfaces — even in direct sunlight.   

 

SEE THE ADVANTAGES